Check icon

Success

Your request has been successfully submitted.

Five Pitfalls of Gas Detection in the Wastewater Industry

The wastewater industry has many confined spaces that contain toxic and/or flammable gases, as well as inert gases that can displace ambient air and create oxygen-deficient environments.

From wet wells and dry wells to digestion and sedimentation tanks, most if not all of these areas qualify as permit-required confined spaces. They demand a vigilant approach to worker safety, including the use of portable gas detectors.

But despite well-publicized safety regulations, recent years have seen more than 100 annual confined-space deaths, with increasing numbers due to chemical inhalations, according to the U.S. Bureau of Labor Statistics.

Here are five common gas safety pitfalls to watch our for:

1. Failure to identify gas threats before starting work.

While working on a pipe valve that was leaking sludge, two mechanics recently died due to high levels of hydrogen sulfide2 — an incident that could have been prevented by air-quality measurements. Remember to always assess the atmospheric conditions of a confined space prior to entry. That typically means using a pumped multi-gas detector to assess the area for oxygen levels; combustible gases, such as methane, at their lower explosive limit; and toxic gases such as hydrogen sulfide and carbon monoxide. If workers take a break from the job, make sure to sample the atmosphere again prior to reentry.

2. Failure to continuously monitor the atmosphere during work.

Atmospheres can change. Just because the air quality in a confined space is deemed safe prior to entry doesn’t mean it will stay that way. Once you determine the atmosphere in a confined space is safe, make sure workers use portable gas detectors as part of their personal protective equipment (PPE) in accordance to their safety training. The detectors will alert workers to rising gas levels so they know to leave the area. No alarm should be ignored.

3. Focusing only on the standard compliance gases.

Safety managers may equip confined-space workers with portable four-gas detectors to monitor the most common gas hazards, including oxygen levels, combustible gases, hydrogen sulfide and carbon monoxide. But these standard compliance detectors are not always sufficient for the wastewater industry, which may include additional hazards such as volatile organic compounds (VOCs), chlorine, ozone or ammonia. If a confined space includes one of these gases, consider providing workers with five-gas portable detectors. The fifth sensor can be configured for the team's needs.

4. Using 9-1-1 as your only rescue plan.

Many safety incidents happen because team leaders focus on reactive response versus proactive monitoring of threats. Therefore, whenever workers are inside a confined space, there should be an attendant outside who uses a pumped detector to continue monitoring changes in gas concentration.

If the attendant sees that a gas level is climbing quickly, he or she can communicate with workers and coordinate evacuation if necessary. Otherwise, if a crew’s only plan is to call 9-1-1 in the event of an emergency, the rescue most likely will not happen in time.

5. Performing hot works without checking for the presence of flammable gas.

In the sludge concentration building at one wastewater treatment plant, several workers were recently injured in an explosion caused by the use of a welding torch around methane gas. To help prevent this kind of incident, use a portable gas detector to monitor the atmosphere for potentially flammable gases — both before and during hot works such as welding and soldering.

Author Image
Alexandra Serban
Content Marketing Specialist
Alexandra Serban is the Content Marketing Specialist for Honeywell Industrial Safety. A seasoned writer and digital storyteller, she is learning and reporting on industrial safety news, trends and products.